Configure general properties of a maintained push button

After you set up the options in the
General
tab, click the
States
tab to specify how the button looks in each state at runtime.
To configure general properties of a maintained push button:
  1. In the
    Maintained Push Button Properties
    dialog box, in the
    General
    tab, specify the following properties if needed:
    • general appearance
    • how the button changes states
    • touch margins
    • audio (whether the button beeps at runtime)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal