Maintained Push Button Properties - General tab
The following table shows options under
Appearance
of the General
tab.Options | Description |
---|---|
Border style | Select the border style. The default style is Line. If the object is a rounded rectangle, circle, or ellipse, the available border styles are None and Line. |
Border width | Type the number of pixels for the width of the object’s border. |
Back style | Select whether the object background is solid, gradient, or transparent. If you select Transparent, the object’s background is not filled in and any objects behind it show through. If you select Gradient, the object's background is filled with a linear gradient color. Specify the color for the background (Back color) in the States tab. |
Shape | Select the shape of the object. If the object is a rounded rectangle, circle, or ellipse, the application applies properties such as size and position by measuring in relation to the object’s bounding box. Tip : Press Ctrl while dragging a corner of the shape to form a square button. |
Corner radius | Available only when the shape is rounded rectangle. Specify how rounded you want the corners to be. |
Border uses back color | Select this check box to use the object’s background color for the border of the button. If this is not selected, you can assign a separate color to the border, instead of using the object’s background color. Specify the background color and the border color in the States tab. |
Highlight color | This field displays the current highlight color. Click it to select another color. For button objects, the button’s border, if any, changes to the highlight color when the operator presses the button at runtime. |
The following table shows options under
State settings
of the General
tab.Options | Description |
---|---|
Next state based on | Select how the button changes states. Current state - the application switches the button from the current state to the other state and writes out the other state value.Value connection - the application reads the value of the Value connection, and, if the value matches one of the button’s state values, changes the button to the other state and writes out the other state value. Select this option if you want the button to base its state on external changes to the Value connection.If the value does not match one of the button’s state values, the application changes the button to State 0 and writes out the State 0 value. |
The following table shows options under
Touch margins
of the General
tab.Options | Description |
---|---|
Touch margins | You can specify a touch-insensitive margin inside the button’s edges. If the operator presses on the touch-insensitive margin, the button press is not registered. |
Horizontal margin | Type the number of pixels for the horizontal touch margin. The horizontal margin is along the button’s left and right edges. |
Vertical margin | Type the number of pixels for the vertical touch margin. The vertical margin is along the button’s top and bottom edges. |
The following table shows options under
Other
of the General
tab.Options | Description |
---|---|
Audio | Select this check box to sound an internal beeper when the object is pressed. If the computer running the project does not have an internal beeper, the object press does not trigger a beep. |
Provide Feedback