Error state for the maintained push button

The error state is shown at runtime if one of the following is true:
  • The
    Value
    connection is unassigned.
  • The value of the
    Value
    connection does not match one of the configured state values.
  • The value of the
    Indicator
    connection does not match one of the configured state values.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal