Data log files are missing after restoring

If data log file sets belonging to an HMI server appear to be missing after restoring, they might not have been included in the backup. The person backing up the HMI server might have chosen to exclude the data file sets to limit the size of the backup and shorten the time required to perform the backup.
Solution:
Add the data log file sets.
  1. Back up the HMI server again, and clear the
    Exclude the data log file sets
    check box.
  2. Restore the HMI server again.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal