Back up an HMI server
Use the HMI Server Backup and Restore utility to back up an HMI server while it is running. To back up an HMI server that is not running, you can use Windows Explorer to copy the files instead of using this utility.
TIP:
To back up an HMI server located on a remote computer, use command line parameters with the HMI Server Backup and Restore utility instead of the graphical user interface.
To back up an HMI server running on this computer:
- In theSelect Operationdialog box, clickBackup HMI Server.
- To save the backup on thelocalcomputer, in theDestination backup pathbox, type or browse for a path to a folder on your computer's local hard disk.
- To save the backup on anetworkcomputer, in theDestination backup pathbox, type or browse for the path to the mapped drive. For details about mapping a network drive, see Windows Help.
Provide Feedback