Backup option
Any data log file sets stored with the HMI server are backed up with it by default.
TIP:
The historical records of DataLogPro will not be backed up with this tool. You need to manually back them up.
If you do not need to restore the data log file sets with the HMI server, and want to limit the size of the backup file and reduce the time necessary to complete the backup, select the
Exclude the data log file sets
check box.If you exclude the data log file sets and want to add them later, you cannot do so without stopping the target HMI server and restoring again. You cannot restore to an HMI server that is running.
Provide Feedback