- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Connection status
OPC/UA Client connection status
- BrowseName
- ConnectionStatusEnum
Values
Value | DisplayName | Description |
---|---|---|
0 | Disconnected | Client is not connected |
1 | Connecting | Client connection is starting |
2 | Connected | Client is connected |
Provide Feedback