Execute an instruction
Instructions execute as part of an active recipe step. They represent the individual steps of a phase. As a batch executes, the current manual instruction for each active step displays. Instructions execute in the order specified within the master recipe.
If you have more than one active recipe step, instructions are displayed for all active
recipe steps.
To locate and execute the instruction
- SelectPrompts.
- (optional) Use theFilterbar to filter and display only the instructions to execute.
- Locate and select the instruction to execute.
- Follow the directions provided in the instruction.
Provide Feedback