Enter report values

Earlier versions of
eProcedure
required that the report values be entered in ALL CAPS. This is no longer the case —
eProcedure
can read the entered value in either upper- or lower-case.
TIP: It is recommended that you include no more than two reports in a single instruction form.
  1. Enter any required report values. Report values can be entered in a text box (field), or you can choose from a list of possible values.
    IMPORTANT: Do not use the following words or phrases as phase parameter names or report parameter names: "all", "length", recipepath", "outerhtml", "finalinstructions", "stepindex", "submitstring", or "submit". Using these phrases as parameter names can cause errors during manual phase control.
ePro_report control step
ePro_ViscosityTestResult
TIP: If there are multiple report values required, be sure to enter all values before clicking the submit button. Once the submit button is clicked the report values are stored in the electronic batch record, and cannot be modified, and the control step is displayed as a past control step.
  1. Click the submit button. (The submit button label can be user-defined; the text could be OK, Submit or Done, but there should be only one submit button per control step.)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal