Confirm report values

Report parameters can be defined to include range checking. The report parameter can require confirmation for values outside a specified range. Report parameters can also be defined to require the report value to be within a specified range, forcing the operator to correct an entry that is outside the range. The
Confirm Value
dialog box is generated from the HTML code.
ePro_client_confirm_value_dialog_box
  • If the report value is valid
    , you can enter an optional comment and then click
    OK
    .
  • If the report value is incorrect
    , click the
    Cancel
    button to cancel the submit process and return to the current control step where the value is selected. You can then enter the correct report value and re-submit the report data.
(See the
eProcedure
Instruction File Design Guide
for information on including Confirm and Comment instructions in control steps.)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal