Phase Status dialog box

The status of a phase can be changed during run time to test phase logic prior to implementation.
  • View parameter tag values and associated parameter names
  • View request tag values
  • Set owner of phase to External
  • Change the phase’s state for phases under External Control
  • Restore active requests for HELD/RESTARTED phases
  • Change report parameter tag values
  • Change value of the Failure bit
  • Set phase to COMPLETE
  • Acknowledge/Clear requests of phases under External control
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal