Phase commands

The
FactoryTalk Batch
Phase Simulator allows you to change the state of a phase. An active phase can be commanded to COMPLETE without gaining phase ownership. All other state change commands require the phase be under external control. The
Start/Stop
,
Abort/Reset
and
Hold/Restart
buttons are modal, in that the command issued is determined based on the phase’s active state at the time the button is clicked. Only legal state change commands are executed. For example, if a phase is RUNNING and the
Start/Stop
button is clicked, the STOP command is issued. START is not a legal command to a phase in the RUNNING state. (Refer to the
FactoryTalk Batch
PCD Programmer Technical Reference Guide
for additional information on legal state transitions.)
This table shows the phase’s transition when the state change command is received, along with the associated state value (
##
).
COMMAND
INITIAL STATE
FINAL STATE
COMPLETE
COMPLETE (70)
START
RUNNING (50)
STOP
STOPPING (30)
STOPPED (80)
ABORT
ABORTING (10)
ABORTED (90)
RESET
IDLE (100)
HOLD
HOLDING (20)
HELD (60)
RESTART
RESTARTING (40)
RUNNING (50)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal