Command a phase
The
FactoryTalk Batch
Phase Simulator allows you to change the state of a phase. To command a phase
:- Start the.FactoryTalk BatchPhase Simulator
- In theEditmenu, selectPhase Status.
- In theSelect Phaselist, select the phase to command.
- To set the phase to COMPLETE, selectSet Complete.
- For all other state change commands, set theOwnerof the phase to External.
- Select the appropriate state change command (Start/Stop,Abort/Reset, orHold/Restart).If the requested state change is legal, the server sends the command and the phase transitions to the appropriate state. The new state value is displayed in theStatusregister in thePhase Statusdialog box.
- If the phase is running andAbort/Resetis selected, the phase goes to ABORTING. To transition the phase to the ABORTED state, selectSet Complete.
- If a phase is running andHold/Restartis selected, the phase goes to HOLDING. To transition the phase to the HELD state, selectSet Complete.
Provide Feedback