Change ownership of a phase
The
Owner
button acts as a toggle, switching the value in the Owner
register between zero and one. A zero represents Batch as the owner and a one represents an external owner.To change ownership of a phase
:- Start the.FactoryTalk BatchPhase Simulator
- SelectEdit > Phase Status.
- From theSelect Phaselist, select the appropriate phase.
- To set ownership toExternal, selectOwnerwhen the value in theOwnerregister is0.To set ownership toBatch, selectOwnerwhen the value in theOwnerregister is1.
Provide Feedback