Acknowledge and clear a request

Requests must be acknowledged and then cleared to allow a phase to continue processing when running under External control. The
Ack/Clear Request
button must be clicked twice, first to acknowledge the request, then to clear the request.
To acknowledge and clear a request
:
  1. Start the
    FactoryTalk Batch
    Phase Simulator
    .
  2. Select
    Edit > Phase Status
    .
  3. In the
    Select Phase
    list, select the phase to command.
  4. If the
    Request
    register contains a request, select
    Ack/Clear Request
    to acknowledge the request. The value in the
    Request
    register changes to
    10
    , indicating that the request confirmation was received from the Batch Server.
  5. Select
    Ack/Clear Request
    to clear the request. Upon clearing the request, the value in the
    Request
    register changes to
    0
    , indicating that the request was cleared. The phase continues to process.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal