Client interface
The
eProcedure
Client provides a graphical representation of a running batch and its associated data.
TIP:
If the
eProcedure
Client does not
display when you open Internet Explorer, you must set the eProcedure
Client
as your home page. In Internet Explorer, select Internet Options
from the Tools
menu, enter http://[computer name]/
(where [computer name] is the name of the computer where the Client is installed) in the
Home page box, and then click eProcedure
OK
. Do the same for any other user accounts that also
use the eProcedure
Client on the computer.The display is divided into five areas:
Information area, Filter area, View Selection area, User-Defined area,
and Command area
.
Provide Feedback