The
eProcedure
Client

The
eProcedure
Client is a web-based application used to create and command batches. A batch is composed of a combination of process-connected phase logic and instruction files that step you, the operator, through the manual process of producing a batch of product.
The
eProcedure
Client makes use of Microsoft’s Internet Explorer along with Active Server Pages (ASPs). The
eProcedure
Server acts as the process-connected device and provides the information to the web pages seen in Internet Explorer. The
eProcedure
Client has five views that you can access by selecting their respective buttons.
ePro_Client_ScreenSelectionArea
  • Equipment view
    The Equipment view provides a graphical view of your facility’s equipment, and displays run-time information that is relevant to the type of equipment displayed. You can use the predefined hyperlinks to access custom web pages, documents, or applications.
  • Instructions view
    The Instructions view provides the ordered list of control steps for the selected filter. You can view current, past, and/or future control steps, as well as add a comment to a particular control step.
  • Batch List view
    The Batch List view is used to create and command a batch. A batch remains on the batch list until the operator removes it or until the
    FactoryTalk Batch
    Server is re-started with a cold boot command.
  • Procedure view
    The Procedure view provides SFC and table views of the selected batch, unit procedure, or operation. You can command any portion of the batch, from the procedure level down to the phase level.
  • Signature List view
    The Signature List view displays a list of pending signatures and their related commands, report parameters, etc., which are maintained on the
    FactoryTalk Batch
    Server.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal