Open the
eProcedure
Client

The
eProcedure
Client runs in Internet Explorer. The
FactoryTalk Batch
Server and
eProcedure
services should be running prior to opening the Client. If configured properly, Internet Explorer can use the
eProcedure
Client as the home page so that when you open Internet Explorer the
eProcedure
Client opens.
(See the
FactoryTalk Batch
Components Upgrade and Installation Guide
for more information.)
TIP: By default, the
FactoryTalk Batch
Server starts automatically when the computer is started. The
FactoryTalk Batch
Server and
eProcedure
Server must be running before opening the
eProcedure
Client.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal