Help button

The
Help
button accesses user assistance for the
eProcedure
Client and the
eProcedure
ActiveX Controls, depending on the current Client focus, as described below:
eProcedure
Help:
Select the
Help
button in the View Selection area to open the user assistance file for the
eProcedure
Client.
ActiveX Help:
Press the
F1
key while an ActiveX control has focus to open the user assistance file for the
eProcedure
ActiveX Controls.
TIP: If selecting
Help
from the Microsoft Internet Explorer menu bar or pressing
F1
when an ActiveX control does not have focus, the user assistance for Internet Explorer opens.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal