Information area

The Information area displays information regarding the plant’s equipment and the current batches. When one of the buttons is clicked in the View Selection area, the information displayed within the Information area changes accordingly. For example, clicking the
Procedure
button displays the Procedure view. In addition, when the button in the Filter area is clicked, the Information area displays the Filter Selection view.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal