Use Microsoft FrontPage to build instruction files
Microsoft FrontPage must be installed and set up correctly to enable the creation of instruction files. Since you will be using forms for the
eProcedure
instruction files, you must select Page Options
from the Tools
menu, then in the General
tab select Automatically enclose form fields within a form
.
Provide Feedback