Create a blank manual instruction file

The first step in building a manual instruction file is creating a blank manual instruction file with one empty control step.
To create a blank instruction file:
  1. Open Notepad. Notepad opens to a new blank page.
  2. Enter the following tags in the page:
<form>
</form>
From the File menu, select Save. The Save As dialog box opens.
Navigate to the desired location, enter a file name in the File name box followed by .html, select the correct file type, and then click Save. This file can be used as a starting point for all new instruction files.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal