FactoryTalk Batch
Client security

FactoryTalk Batch
View,
FactoryTalk
eProcedure
, Batch View HMI controls, Equipment Editor, and Recipe Editor use
FactoryTalk
Security, which allows security settings to be shared among
FactoryTalk
enabled products across a network or on the same computer.
FactoryTalk
Directory is the infrastructure which contains the security policies defined for
FactoryTalk
Security secured resources.
FactoryTalk Batch
secured resources include Batch Commands, Phase Commands, the Batch View windows, and log ons to
FactoryTalk Batch
components. For a complete list of
FactoryTalk Batch
secured objects and their default security policy settings refer to the
FactoryTalk Batch
Administrator Guide
.
FactoryTalk Batch
product policies are created in the Network Directory when the
FactoryTalk
Services Platform installs. The
FactoryTalk Batch
product polices are used to restrict access to the
FactoryTalk Batch
client components and the features within them. (See the
FactoryTalk
Help for more information.)
The
FactoryTalk
Services Platform installation process:
  • Creates both a
    FactoryTalk
    Local Directory and a
    FactoryTalk
    Network Directory on the computer.
    When the install process finishes, both directories are fully configured and ready for use.
    TIP:
    Security settings are completely separate in the Network Directory and Local Directory. Changes you make to the security settings in the Network Directory do not affect the Local Directory and vice versa.
  • Allows any Windows Administrator user account to log on to either directory.
    The installation process automatically adds the local Windows Administrators group to the
    FactoryTalk
    Administrators group in each
    FactoryTalk
    Directory.
  • Allows any authenticated Windows user to log on to the
    FactoryTalk
    Local Directory.
    The installation process automatically adds all members of the local Windows Authenticated Users group to the
    FactoryTalk
    Local Directory.
  • Allows all new user accounts full access permissions.
    The installation process automatically sets system policies to allow all new user accounts added to either directory full access to that directory by default.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal