Implement security
FactoryTalk
e
ProcedureFactoryTalk Batch View
. (See the FactoryTalk Batch
Administrator GuideThe logged in user should:
- be anFactoryTalkSecurity user or a Windows-linked user
- be a user with rights to all of the buttons
If operators wish to perform a function that is secured, for instance for more information.)
Abort
, they must enter a user name and password, which is checked against the FactoryTalk
Security settings defined in the FactoryTalk
Directory. (See the FactoryTalk Batch
Administrator Guide
IMPORTANT:
instructions. However, instructions can be secured through verification signatures.
FactoryTalk
Security cannot be used to secure e
ProcedureProvide Feedback