Understand eProcedure security
eProcedure
securityThere are distinct differences between the security capabilities of the
FactoryTalk
eProcedure
Client and the FactoryTalk Batch
View:- Command buttons in theeProcedureClient are shown, but disabled, if the user does not have the appropriate permissions.
- TheReactivatebutton on the Instructions view of theeProcedureClient and the StepReactivateStepConfirm policy setting inFactoryTalkDirectory are specific toeProcedure.TIP: Because the ability to secureFactoryTalkeProcedureinstruction files does not currently exist inFactoryTalkSecurity, you can require an electronic signature on Parameter Change to prevent unauthorized users from executing instructions. (SeeElectronic signaturesin thefor more information.)FactoryTalk Batch Equipment EditorUser Guide
Provide Feedback