Configure the eProcedure service
eProcedure
serviceThe for more information.)
eProcedure
Service is installed on the FactoryTalk Batch
Server computer and requires no special configuration. The eProcedure
Service can be configured to start manually by changing the startup type in the Services
dialog box of the Control Panel. (See the FactoryTalk Batch
Administrator GuideProvide Feedback