Tighten security for FactoryTalk Batch Clients
Restrict access to specific features of your individual
FactoryTalk
products. Only users with access can use secured product features. For example, when you set up product policies for
FactoryTalk Batch
, restrict use of the Abort command to specific users. This prevents automated batch
processes from being unintentionally aborted during run time.To configure security for multiple features in
FactoryTalk
, use the Feature Security for Product Policies dialog box. To configure security for the
FactoryTalk Batch
features, refer to the secured product policies defined for the FactoryTalk Batch
Clients. To tighten security for Clients
:- Delete the Windows Authenticated Users group from the Local Directory.
- Create newFactoryTalkuser accounts and groups in theFactoryTalk Directory. Create user accounts or groups to secure theFactoryTalk BatchClients.
- Add user accounts and groups created in Windows to theFactoryTalk Directory. Windows accounts added to theFactoryTalk Directoryare called Windows-linked user accounts and groups.IMPORTANT:Windows Workgroup User Accounts are not supported inFactoryTalk.If you use Windows workgroups, you cannot administer user accounts centrally forFactoryTalk BatchClient applications.FactoryTalk Directorydoes not allow multiple user accounts to have the same name and password.
- Remove the All Users group from theFactoryTalk Batchproduct policies. TheFactoryTalkServices Platform installation process adds the All Users group to allFactoryTalkproduct policies.
- Add user accounts and groups to theFactoryTalk Batchproduct policies. To secureFactoryTalk Batchresources, add only the necessary user accounts and groups to the corresponding product policies.
Provide Feedback