Security for FactoryTalk Batch commands

Configure
FactoryTalk
Security to require user confirmation for batch commands and phase commands. A command that has the confirm feature enabled does not execute until the user account is validated in the
Log on to Confirm User
dialog box.
To enable the Confirm feature, configure the
FactoryTalk Batch
product policy for the command and then set the associated <
Command
>
Confirm policy setting to True. These policy settings are defined in
FactoryTalk Directory
for each command button within
FactoryTalk Batch View
and every phase command issued from the
Phase Control
window.
TIP:
When the Confirm feature is enabled for a command, only active user accounts assigned to the Command are allowed to execute the command. Users validated in the
Log on to Confirm User
dialog box are not logged on to
FactoryTalk Directory
.
The <
Command
>
Confirm
policy settings are found in the following locations:
  • FactoryTalk Directory
    \Local | Network\System\Policies\Product Policies\Batch\BatchView and ActiveX\Commands
  • FactoryTalk Directory
    \Local | Network\System\Policies\Product Policies\Batch\BatchView and ActiveX\Phase Commands
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal