Edit the user.asp
The
User.asp
file is located in the \Program Files\Rockwell Software\Batch\web
directory on the FactoryTalk Batch
Server computer. You can modify this file to support requirements specific to your system. For example, you could add HTML code to the User.asp
that links eProcedure
to displays of other manufacturing applications, such as status information from a SCADA (supervisory control and data acquisition) system. The User.asp
can be modified so that documents are always available (because they are not related to specific equipment). You can also modify the User.asp
to specify a timeout period for the Batch List ActiveX control. (For more information on specifying the timeout period, see Specifying the timeout period later in this chapter.)
IMPORTANT:
Do
not
edit any ASPs
other than User.asp
. They are directly related to the successful operation of eProcedure
Other documents could be maintenance schedules, quality lab schedules, personnel shift schedules, pages for e-mail sent to the area, or web mail e-mail sender pages (to allow the operator to send e-mail from the area). You could even point them to stock pages, where the company’s stock price and press releases are posted. You could also add HTML that displays buttons linking to other manufacturing applications like an HMI or LIMS (laboratory information management systems).
Provide Feedback