Add a greeting to the user.asp

You can even add logic to the
User.asp
. The following example adds a greeting based on the time of day.
ePro_User_asp_Greeting
If a user logs onto the
eProcedure
Client after midnight and before noon, the greeting is "Good Morning!" At any other time the user is greeted with "Hello!"
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal