Specify the timeout period

In the
User.asp
file, you can specify the timeout period for the BatchList ActiveX control. The default value is 60000 milliseconds, which equals 60 seconds. If batch creation is taking longer than 60 seconds, you can increase the value as needed. The following example highlights the line you must modify in the
User.asp
file.
ePro_userasp_timeout
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal