ActiveX controls
eProcedure
uses ActiveX controls to communicate with the FactoryTalk Batch
Server and allows you to monitor and interact with control recipes. These controls are necessary for the correct operation of the program. You can specify the timeout period for the batch list ActiveX control to allow for larger batches to be put on the batch list without timing out. You can also embed additional ActiveX controls in HTML recipe forms containing SOPs, which gives you even more flexibility when running a batch recipe with eProcedure
.Provide Feedback