Security Considerations for FactoryTalk Analytics GuardianAI

When deploying FactoryTalk Analytics GuardianAI within operations considerations should be applied to the physical and cyber system security posture of the system. The FactoryTalk Analytics GuardianAI application is designed to run on a client supplied edge hardware and infrastructure.
System security is a paramount tenet of overall operation success. The following document and links are being provided as guidance on best practices of how to implement system security principles within industrial automation control systems. It is of best practice for users of FactoryTalk Analytics GuardianAI to follow these practices to provide the best level of defense in depth security for their overall systems.
Security Publications
Publication Name
Description
Link
Converged Plantwide Ethernet (CPwE) Design
Converged Plantwide Ethernet Design Implementation Guide
Deploying Firewalls within CPwE Architecture
Use cases for designing, deploying, and managing industrial firewalls
Deploy Identity and Mobility Services
Guidelines for protecting systems through deploying centrally managed defense in-depth security approach
Secure Cloud Connectivity to CPwE
Application guide for securing cloud applications within CPwE Architecture
Secure Cloud Connectivity to CPwE
Deploy CIP Security within CPwE
Network security use cases for CPwE systems
Deploy CIP Security within CPwE
IEC 62443 security architecture use cases and design principles
Physical Infrastructure within CPwE Architecture
Use cases for deploying robust physical infrastructure for industrial applications
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal