Network Security and Segmentation
Network security practices within Converged Plantwide Ethernet define the usage of zones and
conduits to segment components within an industrial automation control system. When using
FactoryTalk Analytics GuardianAI it is suggested to follow the CPwE Design Implementation
guide (Converged Plantwide Ethernet Design) to isolate PowerFlex Drives
into various zones. Furthermore, augmenting these zones and conduits with enhanced physical
security is also a best practice as defined by Physical Infrastructure within CPwE
architecture (Physical Infrastructure within CPwE Architecture).
Provide Feedback