Data Integrity and Confidentiality
There is no explicit data or configuration that is shared with FactoryTalk Analytics
GuardianAI. The only information exchanged between the PowerFlex Drive and FactoryTalk
Analytics GuardianAI application is the three electrical phase currents and the electrical
frequency. The user of the FactoryTalk Analytics GuardianAI application is responsible for
protecting the container runtime environment.
Provide Feedback