Denial of Service

The FactoryTalk Analytics GuardianAI application is a small edge run application that only monitors information from PowerFlex drives to provide users insights about electromechanical anomalies and deviations. The application is intended to be run only on internal networks protected by defense-in-depth security as defined by CPwE (Converged Plantwide Ethernet Design). There is no intelligent load balancer built into this application. The user is responsible for guarding against denial-of-service attacks.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal