HART Device Information view
The
HART Device Information
view displays configuration information about the attached HART Field Device.Use the to:
HART Device Information
view- View manufacturer and revision information
- View tag, message, and other descriptor information entered into the HART Field Device
- Check ranges and Primary Variable configuration
- Refresh the device informationTIP:The parameters are not available when offline or HART is not enabled for the channel.
Provide Feedback