Configure HART device information
Use
Set Device Information
to configure the tag name, descriptor and message.Prerequisites
- Verify that you are online and not in Run mode.
To configure HART device information
- On the tab for the device, expandChannels, and then expandChX.
- SelectHART Device Information.
- In theHART Device Informationview, selectSet Device Information.
- (optional) InSet Device Information, selectCopy from Deviceto copy and display the tag, message, and descriptor from the HART device.
- Customize these parameters as needed:TIP:The values must include digits 0 to 9, uppercase letters A to Z, and common punctuation characters.
- TagA short name to identify the HART device. The name may contain a maximum of eight characters.The tag name is displayed in the asset management software, on Handheld HART communicators, and in theHART Device Informationview.
- MessageAdditional information about the device, such as the location of the device or service history. The message can contain maximum of 32 characters.
- DescriptorAdditional information that may be used by the plant or asset management software to identify the HART device. The descriptor can contain a maximum of 16 characters.
- SelectSetto write the tag, message, and descriptor to the HART device.
Provide Feedback