Configuring containers
A container is some type of storage that holds materials. Some containers, such as a bin or tank, hold one material, while others, such as a pallet, can hold multiple materials. Containers can be a source for materials (adding materials from the container) or the destination for materials (such as the distribution of a finished product).
From the
Containers
tab you can add or remove source containers, by
location or individually, to the material’s Configured Containers
list. When you distribute the material you select a container from the list. Only the
containers configured to hold the lots of this material are used in the execution of a
recipe.If the containers are not configured, the
Source Containers
list
only displays the virtual container. There are two methods you can use to configure
containers:- Create the containers first, create the materials second, and then assign containers to materials.
- Create materials first and assign them to the virtual container. As you create the containers, reassign the materials. (See Configuring storage containers for more information.)
Provide Feedback