Assigning containers to materials

  1. From the
    Edit Material
    dialog, select the
    Containers
    tab.
    FTBMM_ED_odin_edit_material_containers
  2. There are three methods you can use to move containers from the
    Source Containers
    list to the
    Configured Containers
    list.
    • To add a storage location of containers, select a location from the
      Source Containers
      list, and then click the
      Add Location
      button. All the containers assigned to that location are added to the
      Configured Containers
      list.
    • To add an individual container, expand the location group to display the containers assigned to that location. Select an individual container, and then click the
      Add
      button.
    • To add all the source containers to the configured containers, click the
      Add All
      button.
  3. Click
    Apply
    to save the changes, or click
    OK
    to save the record and close the dialog.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal