Removing a container
Removing a container merely unassigns the material from that container. The container definition still exists in the material database.
- There are three methods you can use to move containers from theSource Containerslist to theConfigured Containerslist.
- To remove a single container, select the container in theConfigured Containerslist, and then click theRemovebutton.
- To remove more than one container, select the container in theConfigured Containerslist, hold down either theShiftkey or theCtrlkey, select other containers to remove, and then click theRemovebutton.
- To remove all the containers in theConfigured Containerslist, click theRemove Allbutton.
- ClickApplyto save the changes, or clickOKto save the record and close the dialog.
Provide Feedback