Points view
Use the
Points
view to:- For input devices, configure the filter time from Off to On or from On to Off.
- For output devices, determine the behavior of each output when the controller’s mode changes to fault or program. If supported, enable these parameters as needed:
- No Load Detection
- Latch Faults
- Auto Restart
Provide Feedback