Points view parameters (output devices)

The
Points
view for output devices includes these parameters:
TIP:
These parameters are not available in Run mode.
Parameter
Description
Point
Displays the point number to which this configuration applies.
Output State During
Program Mode
Determines the behavior of each output when the controller transitions program mode.
Available values are:
  • Off
    (default)
  • On
  • Hold
Output State During
Fault Mode
Determines the behavior of each output when communication with the controller fails.
Available values are:
  • Off
    (default)
  • On
  • Hold
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal