Points view parameters (input devices)

The
Points
view for input devices includes these parameters:
Parameter
Description
Point
Displays the point number to which this configuration applies.
Input Filter Time
Indicates Off to On or On to Off transition filter constant.
A high signal must be present for this amount of time before the device reports an On.
A low signal must be present for this amount of time before the device reports an Off.
Enter the value in milliseconds (ms). The valid range is from 0.000 through 65.535. The default is 1.000 ms.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal