Search
PointMax Analog HART I/O Modules
Analog HART Input Modules
Analog HART input modules convert an analog signal to a digital value. For example, the modules can convert the following:
Volts
Milliamps
Rolling Timestamp of Data
Module Data Quality Reporting
Multiple Input Ranges
Notch Filter
Digital Filter
Process Alarms
Rate Alarm
Sensor Offset
Open Wire Detection
Field Power (SA Power) Loss Detection
Overcurrent Detection
Underrange/Overrange Detection
Fault and Status Reporting
Calibration
Provide Feedback
Have questions or feedback about this documentation? Please
submit your feedback here
.
Normal