Field Power (SA Power) Loss Detection

The Field Power Loss Detection feature monitors for the loss of field-side power on the SA power bus. It has a corresponding channel level tag that can be examined in the user program if a fault occurs. When field power to the module is lost, the channel level field power loss bit and fault bit are set for all channels and sent to the controller.
IMPORTANT: When SA power drops below 10V, it is possible that you may encounter a rise in the analog input data. You can use the Rate Alarm to monitor the data change rate and discard the input data when Rate Alarm is set.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal