Multiple Input Ranges
The analog HART input module supports multiple input ranges. The input type that you
choose during module configuration determines the available input ranges. An input type
is chosen on a channel-by-channel basis.
Input Type | Available Input Range |
|---|---|
Current (mA) |
|
Voltage (V) |
|
See Chxx view under chapter 5034-IF4IH Details for information on choosing an input
range.
Provide Feedback