Rolling Timestamp of Data

Rolling timestamp represents the time when the current
I.Chxx.Data
is sampled. It is a continuously running 15-bit rolling timestamp that counts in milliseconds from 0…32,767 ms. The rolling timestamp value is reported in the
I.Chxx.RollingTimestamp
tag for the analog I/O modules.
The controller program uses the last two rolling timestamp values to calculate the amount of time between the samples.
A system time change can cause a slight change in input sample timing. The rolling timestamp accurately reflects the change. There can be jitter in the timing between samples before and after the system time change.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal