Manage data logs
Use the
<controller-name>: Manage data log
page to do the following actions:- Fetch data logs for a specified time range from the memory card when the memory card is detected.
- Fetch data logs for a specified time range from the computer when the controller is offline.
- Delete data logs for a specified time range from the memory card.
- Export the data logs to an XLSX or ZIP file to your computer.
Provide Feedback