Change the controller type
Use the
Change Controller
dialog box to change a controller to another controller or revision within the same platform (for example, changing from a 1769-L33ER controller to a 1769-L36ERM controller), or to another platform (for example, from a 1756-L71 controller to a 1769-L33ER controller). The tasking model and instruction usage settings are available only when you use a P-controller. When changing controllers, the project must use a P-controller to access these two P-controller options. The tasking model option is enabled by default unless the existing project was changed to a P-controller from another controller type.
For information about Add-On Instructions, refer to the
Logix5000 Controllers Add-On Instructions Programming Manual
, publication 1756-PM010.Changing from a standard controller to a safety controller (or vice versa) generally affects:
- Supported features
- Physical configuration of the project (safety partner and Safety I/O)
- Controller properties
- Project components such as tasks, programs, routines, and tags
- Safety Add-On instructions
To change the controller type:
- Select the controller, right-click, and selectProperties.
- In theController Propertiesdialog box,Generaltab, selectChange Controllerto open theChange Controllerdialog box.
- InType, select another controller.
- InSoftware Version, select a version number.The list includes only the available controller types and software versions.
- ClickOK.
- Read the dialog box that describes how changing the controller affects the project. ClickYesto change the controller type. ClickNoto keep the current controller type.For a list of the effects of changing from one controller to another, refer to the applicable change scenario:
Provide Feedback